This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: TMS320F28035 ADC采样问题

Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#define SYSCLK 60E6 // 60MHz system clock
#define PWMFREQ 100E3 // 100kHz PWM frequency
#define DUTY_CYCLE 0.20// duty cycle
#define DEAD_BAND 0 // dead band
#define TB_PERIOD (SYSCLK / PWMFREQ) // Calculate period for up-down count mode to 100khz
//#define TB_PERIOD (SYSCLK / (2 * PWMFREQ)) // Calculate period for up-down count mode
//#define TB_PERIOD (SYSCLK / (4 * PWMFREQ)) // Calculate period for up-down count mode
#define DUTY_VALUE (TB_PERIOD * DUTY_CYCLE)
#define DB_VALUE (TB_PERIOD * DEAD_BAND)
//*********************************************************************
__interrupt void adc_isr(void);
void Adc_Config(void);
// Global variables used in this example:
Uint16 LoopCount;
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

代码在生成pwm波形的基础上,加入了基于官方例程Example_2803xAdcSoc修改而来的代码。

代码的目的是通过输入电压来改变pwm的占空比,所以需要先将pwm的代码和adc采样代码合并在一起。

adc和pwm代码作为两个独立的程序运行时是没问题的。但是两个程序合并之后adc代码就不正常了,采样值高达几万。pwm程序是正常的。

我感觉是主程序的问题:

void main(void)
{
InitSysCtrl(); // 初始化系统时钟和PLL

SetGpio(); // Initialize GPIO

DINT; // 禁止所有中断

InitPieCtrl(); // 初始化和启用CPU PIE

IER = 0x0000;
IFR = 0x0000;

InitPieVectTable(); // 初始化PIE向量表

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // 停止所有ePWM时钟
EDIS;

SetEPWM1(); // 初始化ePWM1
SetEPWM2(); // 初始化ePWM2

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // 启动所有ePWM时钟
EDIS;

EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers

//
// Step 4. Initialize all the Device Peripherals:
//
InitAdc(); // For this example, init the ADC
AdcOffsetSelfCal();

PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM

LoopCount = 0;
ConversionCount = 0;


EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 2; // setup EOC2 to trigger ADCINT1 to fire
AdcRegs.ADCSOC0CTL.bit.CHSEL = 1; //set SOC0 channel select to ADCINA1(dummy sample for rev0 errata workaround)
AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1
AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
AdcRegs.ADCSOC3CTL.bit.CHSEL = 3; //set SOC3 channel select to ADCINA3
AdcRegs.ADCSOC4CTL.bit.CHSEL = 4; //set SOC4 channel select to ADCINA4
AdcRegs.ADCSOC5CTL.bit.CHSEL = 6; //set SOC5 channel select to ADCINA6

AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 9; //set SOC0 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 9; //set SOC1 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 9; //set SOC2 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 9; //set SOC3 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 9; //set SOC4 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC5CTL.bit.TRIGSEL = 9; //set SOC5 start trigger on EPwm3A, due to round-robin SOC0 converts first then SOC1, then SOC2

AdcRegs.ADCSOC0CTL.bit.ACQPS = 6; //set SOC0 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6; //set SOC1 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC2CTL.bit.ACQPS = 6; //set SOC2 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC3CTL.bit.ACQPS = 6; //set SOC3 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC4CTL.bit.ACQPS = 6; //set SOC4 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)
AdcRegs.ADCSOC5CTL.bit.ACQPS = 6; //set SOC5 S/H Window to 7 ADC Clock Cycles, (9 ACQPS plus 1)

EDIS;

//
// Assumes ePWM1 clock is already enabled in InitSysCtrl();
//
EPwm3Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm3Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm3Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm3Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm3Regs.TBPRD = 0xFFFF; // Set period for ePWM1
EPwm3Regs.TBCTL.bit.CTRMODE = 0; // count up and start

//
// Wait for ADC interrupt
//
for(;;)
{
LoopCount++;
}

}

不知道是不是配置的步骤有问题还是怎么的,求大神帮忙看一下。