This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simulink_C2000中的tlc文件问题



   在TI给的Simulink实例中,提供了基于两种基于不同tlc文件的Demo。

   请问idelink_ert.tlc和ert.tlc两种文件有什么区别啊?

   为什么用ert.tlc可以正常生成可执行代码,用idelink_ert.tlc就不可以?

  • 楼主,我也是这样的,idelink_ert.tlc总有error,ert.tlc就正常生成,我看matlab论坛说是:

    2. Using idelink_ert.tlc: this is old way of supporting target hardware. New processors are not supported with this system target file.

    If you are new to C2000 support package it is better to use ert.tlc system target file

    请问楼主对这个有什么新的理解么?
  • 但是比如像idelink_ert.tlc就可以设置芯片晶振什么的,ert.tlc就没这个选项,比如搭simulink模型时用epwm模块,我就不清楚他晶振到底会是如何设置的