Other Parts Discussed in Thread: REF35
您好:
ADC采样我使用内部3.3V参考电压,采样窗口设置为10.现在的采样值比实际值偏小5%左右,我使用两块不同的开发板测试结果都一样。
1.是不是因为内部参考电压不准?如果使用REF35芯片提供外部电压,采样值就会准吗?
2.如果采用外部3V参考电压,ADC输入电压为3V时对应4095?如果采用2.5V外部参考电压,ADC输入电压为2.5V时对应4095?

3.我需要对交流电压采样,如果采用2.5V作为外部参考电压,交流电压是不是可以和1.25V的基准电压进行比较,大于1.25V是正半周,小于1.25V是负半周?