Part Number: TMS320F28384S
Other Parts Discussed in Thread: C2000WARE
运行C2000Ware中的点灯例程,如果将CM程序编译为RAM模式,全速或者单步跟踪执行都没有问题,如果编译为flash模式进行调试,单步执行时会出现如下错误信息,请问该错误产生的原因可能是什么?
Cortex_M4_0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.8.0.00235)