This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: tiobj2bin生成Bin文件尺寸不正常

Part Number: TMS320F280025


有2个采用280025的项目,都是采用相同的cmd文件

现在有问题的项目(暂称项目a)之前都能生成正常尺寸的bin文件(56KBytes),现在生成的文件尺寸(1006kbytes)

另外一个项目b能正常生成56Kbytes尺寸的bin文件。

比较了2个项目的cmd文件,完全相同,比较了2个项目的C2000 Compiler参数,C2000 Linker参数,都是相同的

Post-build steps参数也是相同的。

现在搞不清楚到底哪里还能影响到生成bin文件的尺寸

请专家帮忙看看

程序内容存于指定扇区(0x00082000 ~ 0x00088fff):

超大尺寸bin文件内容描述:

文件头部一直到0x000ED7FF的区域全部为0

0x000ED800开始的数据为真正的程序内容,对应FLASH扇区地址为0x00082000:

文件尾部最后一个字节在0x000FB7FF

bin文件中有效数据的尺寸 = 0x000FB7FF - 0x000ED800 + 1 = 0xE000 (Bytes) = 0x7000 (16-bits Words),

刚好能对应(0x00082000 ~ 0x00088fff)的范围