This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用TPS767D301 作为28335内核与IO口供电芯片的问题?



当用TPS767D301 作为28335内核与IO口供电芯片的时候为什么,内核电压与IO口电压之间要并联一个肖特基二极管?

网上给出的解释是:保护 DSP,我看到VDDIO输入电压最大范围-0.3V到2.5V,VDD最大范围为:-0.3V到4.6V。当VDDIO电压为正的很高,或者VDD为负的很高这个肖特基二极管不就没保护作用了吗,能不能帮我详细解释一下,谢谢!