Part Number: TMS320F280039C
工程师好,
如以下代码红色部分,在配置时钟后增加Memcpy函数,重新拷贝至RAM,这个时候其执行时间才有900us,而前一个Memcpy函数执行时间却是30ms,想知道为什么会有这种差异,900us
执行时间的Memcpy函数是否真的拷贝成功了呢?
void Device_Init(void)
{
//
// Disable the watchdog
//
SysCtl_disableWatchdog();
#ifdef _FLASH
//
// Copy time critical code and flash setup code to RAM. This includes the
// following functions: InitFlash();
//
// The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart symbols
// are created by the linker. Refer to the device .cmd file.
//
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); //测试此函数执行时间约30ms
//
// Call Flash Initialization to setup flash waitstates. This function must
// reside in RAM.
//
Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES); // InitFlash();
#endif
//
// Set up PLL control and clock dividers
//设置晶振源
SysCtl_setClock(DEVICE_SETCLOCK_CFG);
//
// Make sure the LSPCLK divider is set to the default (divide by 4)
//
SysCtl_setLowSpeedClock(SYSCTL_LSPCLK_PRESCALE_4);
//
// These asserts will check that the #defines for the clock rates in
// device.h match the actual rates that have been configured. If they do
// not match, check that the calculations of DEVICE_SYSCLK_FREQ and
// DEVICE_LSPCLK_FREQ are accurate. Some examples will not perform as
// expected if these are not correct.
//
ASSERT(SysCtl_getClock(DEVICE_OSCSRC_FREQ) == DEVICE_SYSCLK_FREQ);
ASSERT(SysCtl_getLowSpeedClock(DEVICE_OSCSRC_FREQ) == DEVICE_LSPCLK_FREQ);
#ifndef _FLASH
//
// Call Device_cal function when run using debugger
// This function is called as part of the Boot code. The function is called
// in the Device_Init function since during debug time resets, the boot code
// will not be executed and the gel script will reinitialize all the
// registers and the calibrated values will be lost.
// Sysctl_deviceCal is a wrapper function for Device_Cal
//
SysCtl_deviceCal();
#endif
//
// Turn on all peripherals
//
Device_enableAllPeripherals();
//
// Lock VREGCTL Register
// The register VREGCTL is not supported in this device. It is locked to
// prevent any writes to this register
//
ASysCtl_lockVREG();
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); //测试此函数执行时间约900us,为什么这里重新拷贝至RAM的执行时间那么少,想知道这里是否拷贝成功了?
//
// Configure GPIO20 and GPIO21 as digital pins
//
// GPIO_setAnalogMode(20U, GPIO_ANALOG_DISABLED);
// GPIO_setAnalogMode(21U, GPIO_ANALOG_DISABLED);
}
期待您的回复,感谢!