之前用0049控制电机马达一直正常,移植到0039后开始出现电机转速抖动现象,分析是AD采样问题。两个系列的ADC有什么不同和转移事项吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,关于这两个型号芯片之间的移植你可以参考下这个文件:
移植的话需要根据上面我发的文件来移植。如果ADC没有差别的话,那么实际情况不一样也可能是一些其他工程里面的移植细节没有注意到而导致的。具体是那一方面我无从得知,需要根据您的工程以及实际情况来分析。
重新画了板子,现象还是一样,下面是ADC的初始化程序,帮忙看下是否有错误
void InitSetAdc(Uint type)
{
volatile Uint waite;
int trigsel;
trigsel = 5;
//EALLOW;
#define ANALOGSUBSYS_BASE 0x0005D700U
ADC_setVREF(ANALOGSUBSYS_BASE, 0, 0);
//AnalogSubsysRegs.ANAREFCTL.bit.ANAREFSEL = 0; // 内部基准,1.65(0~3.3V)
//AnalogSubsysRegs.ANAREFCTL.bit.ANAREFBSEL = 0;
//AnalogSubsysRegs.ANAREFCTL.bit.ANAREFCSEL = 0;
EALLOW;
AdcaRegs.ADCCTL2.bit.PRESCALE = 0x02;
AdcbRegs.ADCCTL2.bit.PRESCALE = 0x02;
AdccRegs.ADCCTL2.bit.PRESCALE = 0x02;
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; //All analog circuitry inside the core is powered up
AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
AdccRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//============================================================================================
//复位
for(waite = 0;waite<5000;waite++){} //延时
//------------------------------------------------------------------------------------------------
asm(" RPT #28 || NOP"); // 需延时两个ADCCLK;延时28个空周期
//以下开始设置ADC的控制寄存器、转换通道选择寄存器等
AdcaRegs.ADCBURSTCTL.bit.BURSTEN = 0; // SOC Burst Mode Enable
AdcbRegs.ADCBURSTCTL.bit.BURSTEN = 0; // SOC Burst Mode Enable
AdccRegs.ADCBURSTCTL.bit.BURSTEN = 0; // SOC Burst Mode Enable
//AdcaRegs.ADCOFFTRIM.all = 0;
//AdcbRegs.ADCOFFTRIM.all = 0;
//AdccRegs.ADCOFFTRIM.all = 0;
AdcbRegs.ADCINTSEL1N2.bit.INT1SEL = 4; // 通道3转换完成产生中断ADCINT1
if (0 == type)
{
AdcbRegs.ADCINTSEL1N2.bit.INT1E = 1; // ADCINT1 is enabled
}
else
{
AdcbRegs.ADCINTSEL1N2.bit.INT1E = 0; // ADCINT1 is disabled
}
AdcbRegs.ADCINTOVFCLR.bit.ADCINT1 = 1;
#define ADC_IW_A2 0x02 // IW A2
#define ADC_AI4_A5 0x05 // AI4 A5
#define ADC_VV_A6 0x06 // VV A6
#define ADC_IU_B2 0x02 // IU B2
#define ADC_VDC_B5 0x05 // VDC B5
#define ADC_AI5_B8 0x08 // AI5 B8
#define ADC_AI6_B9 0x09 // AI6 B9
#define ADC_IV_B11 0x0B // IV B11
#define ADC_UV_C0 0x00 // UV C0
#define ADC_AI1_C2 0x02 // AI1 C2
#define ADC_TD_C3 0x03 // TD C3
#define ADC_WV_C4 0x04 // WV C4
#define ADC_AI2_C5 0x05 // AI2 C5
#define ADC_ACQPS 2
//********************************ePWM1 ADCSOCA触发,
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcaRegs.ADCSOC2CTL.bit.CHSEL = ADC_IW_A2; // 18:15 SOC0 Channel Select
AdcaRegs.ADCSOC0CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
/*
AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcaRegs.ADCSOC1CTL.bit.CHSEL = ADC_IW_A2; // 18:15 SOC0 Channel Select
AdcaRegs.ADCSOC1CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcaRegs.ADCSOC2CTL.bit.CHSEL = ADC_IW_A2; // 18:15 SOC0 Channel Select
AdcaRegs.ADCSOC2CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcaRegs.ADCSOC3CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcaRegs.ADCSOC3CTL.bit.CHSEL = ADC_IW_A2; // 18:15 SOC0 Channel Select
AdcaRegs.ADCSOC3CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
*/
AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcaRegs.ADCSOC1CTL.bit.CHSEL = ADC_AI4_A5; // 18:15 SOC0 Channel Select
AdcaRegs.ADCSOC1CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcaRegs.ADCSOC0CTL.bit.CHSEL = ADC_VV_A6; // 18:15 SOC0 Channel Select
AdcaRegs.ADCSOC2CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcbRegs.ADCSOC0CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC2CTL.bit.CHSEL = ADC_IU_B2; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC0CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
/*
AdcbRegs.ADCSOC1CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC1CTL.bit.CHSEL = ADC_IU_B2; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC1CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcbRegs.ADCSOC2CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC2CTL.bit.CHSEL = ADC_IU_B2; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC2CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcbRegs.ADCSOC3CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC3CTL.bit.CHSEL = ADC_IU_B2; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC3CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
*/
AdcbRegs.ADCSOC1CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC1CTL.bit.CHSEL = ADC_VDC_B5; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC1CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcbRegs.ADCSOC2CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC0CTL.bit.CHSEL = ADC_AI5_B8; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC2CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcbRegs.ADCSOC3CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC3CTL.bit.CHSEL = ADC_AI6_B9; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC3CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdcbRegs.ADCSOC4CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCSOC4CTL.bit.CHSEL = ADC_IV_B11; // 18:15 SOC0 Channel Select
AdcbRegs.ADCSOC4CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdccRegs.ADCSOC0CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdccRegs.ADCSOC0CTL.bit.CHSEL = ADC_UV_C0; // 18:15 SOC0 Channel Select
AdccRegs.ADCSOC0CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdccRegs.ADCSOC1CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdccRegs.ADCSOC1CTL.bit.CHSEL = ADC_AI1_C2; // 18:15 SOC0 Channel Select
AdccRegs.ADCSOC1CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdccRegs.ADCSOC2CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdccRegs.ADCSOC2CTL.bit.CHSEL = ADC_TD_C3; // 18:15 SOC0 Channel Select
AdccRegs.ADCSOC2CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdccRegs.ADCSOC3CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdccRegs.ADCSOC3CTL.bit.CHSEL = ADC_WV_C4; // 18:15 SOC0 Channel Select
AdccRegs.ADCSOC3CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdccRegs.ADCSOC4CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdccRegs.ADCSOC4CTL.bit.CHSEL = ADC_AI2_C5; // 18:15 SOC0 Channel Select
AdccRegs.ADCSOC4CTL.bit.ACQPS = ADC_ACQPS; // 8:0 SOC0 Acquisition Prescale
AdccRegs.ADCSOC5CTL.bit.TRIGSEL = trigsel; //ePWM1, ADCSOCA
AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
EDIS;
}
补充下 #define ADC_ACQPS 最大设置到50,都是同样的现象
你有没有注意过你的SOC是在什么时间触发的,有没有和EPWM做同步,如果soc开始的时刻恰好和pwm动作的时刻(开通或者关断)重合,003X的采样是会有异常,这是我观察到的现象
SOC是EPWM上溢和下溢触发的。你说的PWM开通关断影响AD采样是有可能的,因为电机转速低是正常的,电机运行到80%额定转速时就会出现抖动,这时候PWM输出的电压矢量比较大,PWM开通关断是接近于SOC触发点的
参考下工程师的回复:
28034,28335平台都用过没遇到问题
F2803x / F2833x devices are Gen2 devices and the peripherals are quite different compared to F28004x / F28003x devices.
They can review the F28004x to F28003x migration guide below, there may be some important differences they need to account for.