This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H22C: F28M35 Serial Boot(串口启动)

Part Number: F28M35H22C


TI工程师您好,我准备在F28M35器件上正在开发一款串口升级软件,此软件并非内置到Flash中的Bootloader,而是利用器件的M-Boot ROM Serial Boot Mode特性,上电前将BOOT PIN (PG3_GPIO43、PG7_GPIO47、PF3_GPIO35、PF2_GPIO34)分别置为0100,然后在PA0_GPIO0、PA1_GPIO1上连接USB转TTL的TX、RX引脚,通过一个上位机程序将m3的程序下载到m3的ram中去执行,TI的手册中记录了上位机程序和M-Boot ROM的通信协议,并且说了器件有auto baud特性,现在我的问题是,上位机通信接口要进行什么操作,M-Boot ROM才能有反应,无论我怎么做,m3就是没反应,谢谢!