我使用CCSV5.4連接F28035控制卡
並使用controlsuit裡提供的範例"HVACI_Sensorless"
但當我依照"HVMotorCtrl+PFC (R1.1) Kit How to Run Guide "的軟體設置步驟執行到步驟16
debug後出現一個WARNING
=======================================
This project was created using a version of compiler that is not currently installed: 6.0.1 [C2000]. Another version of the compiler will be used during build: 6.1.3. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
=======================================
請問我想在CCSV5.4繼續操作
我該如何解決此WARNING?