Other Parts Discussed in Thread: C2000WARE
编译报错提示
#20 identifier "float32" is undefined 原位置:C:\ti\C2000Ware_DigitalPower_SDK_5_00_01_00\libraries\solar\mppt_pno.h C/C++ 问题
已知这一行定义在“C:\ti\C2000Ware_DigitalPower_SDK_5_00_01_00\c2000ware\device_support\f280015x\headers\include\f280015x_device.h”文件下:
//
// The following data types are included for compatibility with legacy code,
// they are not recommended for use in new software. Please use the C99
// types included above
//
#if (!defined(DSP28_DATA_TYPES) && !defined(F28_DATA_TYPES))
#define DSP28_DATA_TYPES
#define F28_DATA_TYPES
#ifdef __TMS320C28XX_CLA__
typedef short int16;
typedef long int32;
typedef unsigned char Uint8;
typedef unsigned short Uint16;
typedef unsigned long Uint32;
typedef float float32;
typedef long double float64;
typedef struct { Uint32 low32; Uint32 high32; } Uint64;
typedef struct { int32 low32; int32 high32; } int64;
也已将该文件添加入工程的include options中
但是编译“C:\ti\C2000Ware_DigitalPower_SDK_5_00_01_00\libraries\solar\mppt_pno.h”仍然会报错