SPRS880O手册,171页, 章节8.12.6.1.1USB输入端口DP和DM时序要求。这个表格中各个数据的最小值,最大值是通过什么方式测量出来的?具体的测量步骤是什么样的?需要用到哪些工具?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SPRS880O手册,171页, 章节8.12.6.1.1USB输入端口DP和DM时序要求。这个表格中各个数据的最小值,最大值是通过什么方式测量出来的?具体的测量步骤是什么样的?需要用到哪些工具?
你好,参考如下:
根据解释我还有如下问题:
1.VIL最小值是0.8V,VIH最大值是2.0V。是否可以理解为VIL应小于等于0.8V,VIH应大于等于2.0V?
2.VDI最大值是0.2V,是否可以理解为DP电压与DM电压的差值应小于等于0.2V?
3.VCM的计算是否可以用这个公式:(DP电压+DM电压)/2?
4.如果前三个问题是对的,那么如果VCM=0.8V,根据VDI最大是0.2V的要求,则DP电压和DM的电压范围应该为(0.7V~0.9V),如果这样就不满足VIH大于等于2.0V的要求。