This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI团队好:
我使用F28P65x controlCard运行led_ex1_c28x_dual_blinky_cpu1例程,在CPU1程序进入flash模式debug后,配置好CPU1与CPU2 erase flash,然后启动CPU2连接,每次都是只能加载RAM.out程序文件且可正常运行,加载FLASH.out文件将会报如下错误,请问此问题应当如何处理,才可以正确加载CPU2的FLASH程序离线运行呢?
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output:
CPU2 is out of reset and configured to wait boot.
(If you connected previously, may have to resume CPU2 to reach wait boot loop.)
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output:
CPU2 is out of reset and configured to wait boot.
(If you connected previously, may have to resume CPU2 to reach wait boot loop.)
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output:
CPU2 is out of reset and configured to wait boot.
(If you connected previously, may have to resume CPU2 to reach wait boot loop.)
C28xx_CPU2: GEL Output:
RAM initialization done
C28xx_CPU2: GEL Output:
Memory Map Initialization Complete
C28xx_CPU2: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
C28xx_CPU2: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_CPU2: File Loader: Verification failed: Values at address 0x0E0000@Program do not match Please verify target memory and memory map.
C28xx_CPU2: GEL: File: D:\ccs12\led_ex1_c28x_dual_blinky_cpu2\CPU2_FLASH\led_ex1_c28x_dual_blinky_cpu2.out: a data verification error occurred, file load failed.