This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157: ADC的输入电压范围

Part Number: TMS320F2800157


在一个项目中,用ADC对一个模拟信号进行采样,发现模拟信号的电压范围要在0V~3.3V之间,ADC才能正常采样

之前好像有在哪里看到一个资料,说是ADC可以配置,让模拟信号的电压范围是0V~3.3V或者 -1.5V~1.5V

请问是否有这个配置?应该如何配置