This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F2800137: 咨询一下,就是用官方历程flashapi_ex1_programming.c制作一个bootloader程序,或者有没有教程

Part Number: LAUNCHXL-F2800137
Other Parts Discussed in Thread: C2000WARE

修改cmd文件,如下所示,会跳转不到APP地址,

MEMORY
{
   BEGIN            : origin = 0x00080000, length = 0x00000002
   BOOT_RSVD        : origin = 0x00000002, length = 0x00000126

   RAMM0            : origin = 0x00000128, length = 0x000002D8
   RAMM1            : origin = 0x00000400, length = 0x000003F8
   // RAMM1_RSVD       : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RAMLS0           : origin = 0x00008000, length = 0x00002000
   RAMLS1           : origin = 0x0000A000, length = 0x00001FF8
   // RAMLS1_RSVD      : origin = 0x0000BFF8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RESET            : origin = 0x003FFFC0, length = 0x00000002

   /* Flash sectors */
   //FLASH_FLAG      	: origin = 0x081C00, length = 0X4  /* on-chip Flash */
   FLASHIDFLAG     	: origin = 0x081C04, length = 0x4  /* on-chip Flash */
   //USER_FLASH      	: origin = 0x081C08, length = 0X3F8  /* on-chip Flash */
   FLASH_APP      	: origin = 0x082002, length = 0xDFFE//, fill=0xFFFF  /* on-chip Flash */

//   FLASH_BANK0_SEC_0_7     : origin = 0x080002, length = 0x1FFE  /* on-chip Flash */
//   FLASH_BANK0_SEC_8_15    : origin = 0x082000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_16_23   : origin = 0x084000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_24_31   : origin = 0x086000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_32_39   : origin = 0x088000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_40_47   : origin = 0x08A000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_48_55   : origin = 0x08C000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_56_63   : origin = 0x08E000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_64_71   : origin = 0x090000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_72_79   : origin = 0x092000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_80_87   : origin = 0x094000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_88_95   : origin = 0x096000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_96_103  : origin = 0x098000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_104_111 : origin = 0x09A000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_112_119 : origin = 0x09C000, length = 0x2000  /* on-chip Flash */
//   FLASH_BANK0_SEC_120_127 : origin = 0x09E000, length = 0x1FF0  /* on-chip Flash */

   // FLASH_BANK0_SEC_127_RSVD : origin = 0x0A0FF0, length = 0x0010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}

SECTIONS
{
   codestart        : > BEGIN
   codeclearram     : > FLASH_APP
   .text            : > FLASH_APP, ALIGN(8)

   .cinit           : > FLASH_APP, ALIGN(8)
   .switch          : > FLASH_APP, ALIGN(8)

   .reset           : > RESET,  TYPE = DSECT /* not used, */

   .stack           : > RAMM1

#if defined(__TI_EABI__)
   .bss             : > RAMLS0
   .bss:output      : > RAMLS0
   .init_array      : >> FLASH_APP, ALIGN(8)
   .const           : >> FLASH_APP, ALIGN(8)
   .data            : > RAMLS0
   .sysmem          : > RAMLS0
  .bss:cio          : > RAMLS0
#else
   .pinit           : >> FLASH_APP, ALIGN(8)
   .ebss            : > RAMLS0
   .econst          : >> FLASH_APP, ALIGN(8)
   .esysmem         : > RAMLS0
   .cio             : > RAMLS0
#endif

#if defined(__TI_EABI__)
   .TI.ramfunc      : LOAD = FLASH_APP,
                      RUN = RAMLS0,
                      LOAD_START(RamfuncsLoadStart),
                      LOAD_SIZE(RamfuncsLoadSize),
                      LOAD_END(RamfuncsLoadEnd),
                      RUN_START(RamfuncsRunStart),
                      RUN_SIZE(RamfuncsRunSize),
                      RUN_END(RamfuncsRunEnd),
                      ALIGN(8)
#else
   .TI.ramfunc      : LOAD = FLASH_APP,
                      RUN = RAMLS0,
                      LOAD_START(_RamfuncsLoadStart),
                      LOAD_SIZE(_RamfuncsLoadSize),
                      LOAD_END(_RamfuncsLoadEnd),
                      RUN_START(_RamfuncsRunStart),
                      RUN_SIZE(_RamfuncsRunSize),
                      RUN_END(_RamfuncsRunEnd),
                      ALIGN(8)
#endif
   IDFLAG         	 : > FLASHIDFLAG
   DataBufferSection : > RAMLS1, ALIGN(2)
    /*  Allocate IQ math areas: */
   IQmath           : > FLASH_APP, ALIGN(8)
   IQmathTables     : > FLASH_APP, ALIGN(8)
}

通过这个跳转,

会进入这个中断里面