This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35x 的ADCINT与PIE Peripheral Interrupts如何对应?



请问:F28M35x 的ADC1和ADC2各有8个中断,ADCINT1--ADCINT8,通过与门最终只有8个中断进入PIE,它们就是PIE 表中的ADCINT1--ADCINT8,那ADC1的ADCINT1--ADCINT8,和ADC2的ADCINT1--ADCINT8,与PIE的ADCINT1--ADCINT8如何对应?是从ADC1的INT1--INT8排起,再排ADC2的INT1-INT8?还是ADC1 INT1,ADC2 INT1....交叉排?比如ADC1中Enable了ADCINT1,ADCINT2,ADCINT3,ADCINT4,ADCINT5,ADC2中Enable了ADCINT1,ADCINT2,ADCINT3,如何与PIE中的ADCINT1~ADCINT8如何对应?

   另外,PIE Peripheral Interrupts中的INT1.1(ADCINT1)、INT1.2(ADCINT2),与INT10.1(ADCINT1),INT10.2(ADCINT2)是不是重复的,同时只能一个有效?是不是用哪个都行呢?

   还望各位大牛门不吝解答!谢谢!