Other Parts Discussed in Thread: TMDSCNCD28379D
因]第一使用此顆IC, 軟體是CCS Version: 12.2.0.00009 , 燒錄器為Blackhawk USB560 V2 System Trace
完成Build Debug 後, 進入Debug 專案, 馬上出現以下錯誤, 希望尋求協助
C28xx_CPU1: Trouble Writing Register XAR0: (Error -1041 @ 0x7) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation
package 9.10.0.00080)
C28xx_CPU1: GEL: Error while executing OnReset(0): Target failed to write register XAR0
at XAR0=*((unsigned long*) 0x78018) [f28379d_cpu1.gel:421]
at SetupDCSM() [f28379d_cpu1.gel:31]
at OnReset(0)
C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
C28xx_CPU1: Failed CPU Reset: (Error -1041 @ 0x6) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package
9.10.0.00080)
C28xx_CPU1: Error: (Error -1135 @ 0x3FF16A) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.10.0.00080)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you
connect and reload your program before you continue debugging
C28xx_CPU1: GEL: Error while executing OnReset(-1): Could not write 0x0005D122@Data: target is not connected
at *((long int*) 0x5D122)=0xA5A50000 [f28379d_cpu1.gel:28]
at OnReset(-(1))
C28xx_CPU1: GEL: Error calling OnPreFileLoaded(): Reset failed: retcode=-1
C28xx_CPU1: File Loader: Verification failed: Could not write 0x080002@Program: target is not connected
C28xx_CPU1: GEL: File: C:\Users\jorda\workspace_v12\ESP2300\Debug\ESP2300.out: Load failed.