This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28034: 关于Receive Data Sample Timing的要求

Part Number: TMS320F28034

希望知道TMS320F28034这颗料,关于Receive Data Sample Timing的要求是多少?

  • 你好,能否解释一下你说的这个参数是哪方面的参数?这样我可以更好的寻找相关的资料。

  • 您好,是关于通讯方面的。图片是瑞萨RX66T的资料,红色标注部分有相应参数可以提供吗?

  • 我咨询下资深工程师后回复您。

  • 确认一下,您问的是 F2803x SCI 接收容差吗?

  • 应该是没有完全一直的参数,只能是参考手册12.10的内容,下面是工程师的回复:

    I do not know of an SCI specification that matches the parameter in the images you shared. Are you referring to the SCI sampling error tolerance? The SCI module samples using the SCICLK and a 'majority vote' logic as described in the device TRM:

    While there is no spec for this (depends on other variables such as your baud rate, clock dividers, etc.) the SCI clock cycles that surround cycles 4, 5, and 6 in the image above would allow for some error tolerance. Is this information helpful at all to what you are looking for?

  • 感谢您的答复