This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TIDM-02010—dmpfc-0013X的双电机的代码,我只想使用此代码控制一个电机,我将电机1的底层配置(ADC采样,PWM波等)配置成我的芯片需求,其中PFC和电机二底层配置未进行改动;然后进行测试,按照双电机
“具有数字交错式 PFC、适用于 HVAC 的双电机控制参考设计”的手册进行测试,在完成第一部分CPU和电路板设置时,电机1能够发出所设定的PWM波,但在进行V/F测试时,电机电压和电流很小,无法启动电机旋转。请问有更详细的测试文档说明吗?其中我已确认ADC采样基本没有问题,继电器在上电时也顺利闭合,在进行V/F测试时,电机也发出占空比,但电机无法旋转,请说明,重点需要修改什么参数。谢谢
参考下工程师的回复:
You don't need to change anything, just run one motor by enabling the command flag to understand the working flow first. Please take a look at the lab user's guide, you may only need to change the motor control parameters according to your motor.