想要实现epwm1和epwm2之间的同步,我看了280025的手册发现和28335的不太一样,我没看明白到底同步信号是怎么连接的,请问一下到底怎么配置epwm1和epwm2信号同步
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想要实现epwm1和epwm2之间的同步,我看了280025的手册发现和28335的不太一样,我没看明白到底同步信号是怎么连接的,请问一下到底怎么配置epwm1和epwm2信号同步
ePWM type 4引入新的同步策略来增加灵活性。
具体操作分2步:
1.设置epwm1.SYNCOUT的触发逻辑:
例如希望每次CTR=ZERO时触发SYNCOUT,则设置 ZEROEN = 1,OSHTSYNCMODE = 0
如果希望干预触发SYNCOUT的条件,则设置 ZEROEN = 1,OSHTSYNCMODE = 1,
然后在需要触发SYNCOUT时,根据OSSFRCEN位向OSHTLD或OSHTSYNC写1,当CTR=ZERO时,自动触发1次SYNCOUT
2.设置epwm1.SYNCIN的源:
EPWMSYNCINSEL.SEL = 1