This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157: 调用EPWM_setActionQualifierContSWForceAction()函数给PWM输出0/1,此时配置的PWM死区时间还有效吗

Part Number: TMS320F2800157


调用如下的EPWM_setActionQualifierContSWForceAction()函数给PWM输出0/1,相当于用软件的方式控制PWM输出0/1(而不是通过PWM的CMPA/CMPB寄存器的方式),

此时配置的PWM死区时间还有效吗?

//*****************************************************************************
//
//! Triggers a continuous software forced event.
//!
//! \param base is the base address of the EPWM module.
//! \param epwmOutput is the ePWM pin type.
//! \param output is the Action Qualifier output.
//!
//! This function triggers a continuous software forced Action Qualifier output
//! on ePWM A or B based on the value of epwmOutput.
//! Valid values for the parameters are:
//! - epwmOutput
//! - EPWM_AQ_OUTPUT_A - ePWMxA output
//! - EPWM_AQ_OUTPUT_B - ePWMxB output
//! - output
//! - EPWM_AQ_SW_DISABLED - Software forcing disabled.
//! - EPWM_AQ_SW_OUTPUT_LOW - Set output pins to low
//! - EPWM_AQ_SW_OUTPUT_HIGH - Set output pins to High
//!
//! \return None.
//
//*****************************************************************************
static inline void
EPWM_setActionQualifierContSWForceAction(uint32_t base,
    EPWM_ActionQualifierOutputModule epwmOutput,
    EPWM_ActionQualifierSWOutput output)

  • Triggers a continuous software forced event.
    This function triggers a continuous software forced Action Qualifier output

    没有效果。因为DB模块添加死区是通过检测上升沿或下降沿实现的

    而且既然输出已经固定为高或低了,也就不存在死区一说了

  • 前面没有吧2问题描述清楚,我使用的场景是这样的:

    EPWM_setActionQualifierContSWForceAction(High)  ---- PWM初始输出1

    EPWM_setActionQualifierContSWForceAction(Low)    ---- 相当于用软件的方式,吧PWM输出从1变成0,有下降沿,此时死区时间有效吗

    EPWM_setActionQualifierContSWForceAction(High)    ---- 相当于用软件的方式,吧PWM输出从0变成1,有上升降沿,此时区时间有效吗

    EPWM_setActionQualifierContSWForceAction(Low)    ---- 相当于用软件的方式,吧PWM输出从1变成0,有下降沿,此时死区时间有效吗

  • 有效的,正如我上面所说,DB模块添加死区是通过检测上升沿或下降沿、然后在此基础上叠加延迟实现的