This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

關於f28335的ADCREFP&ADCREFM這2隻腳的電位

Other Parts Discussed in Thread: LM4140, TMS320F28335

請問如果是一個全新的晶片(沒燒寫過),這2腳的電位還是應該為0.5v跟1.2v嗎?

如果是的話,我的板子上這2腳為0v應該檢查哪地方呢? (我已檢查過電源跟地的接腳了..)

  • 采样精度的保证,除了ADC自身的指标要好,外部电路的设计抗干扰性好、带宽高以外,参考电压的选择也很关键,因为它也直接决定了ADC采样结果的转换精度。

    默认情况下我们可以选择F28335的ADC自带的片内参考电压作为ADC转换的基准电压,其温度稳定度可以达到~50 PPM/°C。如果不满足要求的话,我们也可以根据需要,通过配置ADCREFSEL寄存器来选择片外参考电压作为基准电压。片外参考电压连接到ADCREFIN引脚上,可选2.048V、1.5V或1.024V。但是无论选择哪种外部参考电压值,ADC采样模块本身的电气特性都限制了ADC输入通道的电压范围只能在0-3V,超过范围则极有可能损坏ADC模块甚至是整个DSP模块(因为CMOS电路过压之后的雪崩击穿会导致芯片永久损坏)。

    如果选择内部参考电压作为转换的基准电压,则ADCREFIN引脚可配置为连接到外部电压、悬空或接地三种模式。而在使用外部参考电压时,无论选择哪种模式,外部引脚ADCRESEXT、ADCREFP及ADCREFM的连接情况都相同。如图1所示为外部参考电压为2.048V时的连接情况。

     

    外部参考电压的精度直接影响ADC的采样精度,所以需要非常稳定的参考芯片,一般情况下使用串联电压源或者线性稳压器LDO。TI自身推出的REF3020就是一个代表,其管脚很少,封装也较小(SOT23-3),价格只有几块钱,非常适合做为高精度的外部参考电压源。几个参考值可以分别用:

    REF3020:2.048V

    LM4140:1.024V

    TLV7015:1.5V

  • TMS320F28335/F28334/F28332/F28235/F28234/F28232 Digital Signal Controllers (Rev. M) 的 Table 6-50. ADC Electrical Characteristics中指出

    VADCREFP - ADCREFP output voltage at the pin based on  internal reference  1.275 V

    VADCREFM - ADCREFM output voltage at the pin based on  internal reference  0.525 V

    我想知道這2個電位 只要3.3V與1.9V上了之後就應該出現的嗎 (跟內部程序沒有關係?)

    我的板子上量測都為0V 可是檢查了所有電源跟地 都沒有接錯...不曉還能檢查那些地方...?

  • 原本沒辦法燒寫flash 所以只能一直檢查硬體 現在莫名其妙可以燒寫了(硬體、軟體都沒動)

    那2隻腳的電位 對於全新的DSP是沒有輸出的...我燒寫過後量測到了