1、程序在RAM和Flash里用仿真器都跑过了,一切正常
2、将程序通过串口bootloder刷进去,也刷成功了,可以看到中断触发的led灯在闪烁,但是部分功能比如串口、CAN通信功能异常;
3、将程序直接通过仿真器刷到Flash里,调试过程是没有问题的,但是重新上下电,通过供电电源,可以看出来,芯片没有正常工作,当然,中断触发的led灯也没有闪烁。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、程序在RAM和Flash里用仿真器都跑过了,一切正常
2、将程序通过串口bootloder刷进去,也刷成功了,可以看到中断触发的led灯在闪烁,但是部分功能比如串口、CAN通信功能异常;
3、将程序直接通过仿真器刷到Flash里,调试过程是没有问题的,但是重新上下电,通过供电电源,可以看出来,芯片没有正常工作,当然,中断触发的led灯也没有闪烁。
最新进展:
1、flash无法重新上电启动,是CMD文件配置问题,已解决;
2、但经过bootloder跳转的程序,经排查,会卡死在定时器1的一条指令上,但是使用仿真器调试没有此问题。(因为一上电,sci那条消息可以发出来,can那条发不出来)
SCI_DataFrame_Tx(&SCI_Frame.Data_Frame_B.Data_Frame1);
//! 主循环定时
while(TIMER_getStatus(halHandle->timerHandle[1]) == TIMER_Status_CntIsNotZero){}//TIMER_Status_CntIsNotZero
ECanaBoxTxMsg(halHandle->canAHandle,&CAN_Frame.TX,0x05);