Part Number: TMS320F280049C
280049在CLA中调用CLAsin,接上仿真器跑时正常,不接仿真器运行时CLAsin结果一直为0.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C
280049在CLA中调用CLAsin,接上仿真器跑时正常,不接仿真器运行时CLAsin结果一直为0.
已解决,将CLA1mathTables : > RAMLS1, PAGE = 1注释,
保留CLA1mathTables : LOAD = FLASH_BANK1_SEC15,
RUN = RAMLS1,
LOAD_START(CLA1mathTablesLoadStart),
RUN_START(CLA1mathTablesRunStart),
LOAD_SIZE(CLA1mathTablesLoadSize),
PAGE = 1, ALIGN(4)
并且在main.c加上memcpy((uint32_t *)&CLA1mathTablesRunStart, (uint32_t *)&CLA1mathTablesLoadStart,
(uint32_t)&CLA1mathTablesLoadSize);
感谢分享~
一般来说,仿真器连接时工作正常、而不连仿真器运行在FLASH时异常,大概率与函数或者代码的搬运有关。