想请问一下,vienna整流器的输入电流是根据负载不同而不同吗?在整流桥中电流范围是多少?峰值电流能到10A吗?输出直流侧的电流范围是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考下工程师的回复:
Does the input current of the Vienna rectifier vary depending on the load? - Yes. example, If adding an inductive load component will also impact the current waveforms.
Current range is mentioned in the design guide:

for the 10A peak. as per design guide it looks possible, whereas the sensing circuit can sense upto 12A. (refer calulation.xlsx sheet in hardware folder)