This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: TMS320F28379D

Part Number: TMS320F28379D

在跑eqep_ex2_pos_speed.c这个例程时,能够正常运行,但我把相关的eqep_ex2_calculation.c中的PosSpeed_calculate()函数放进我自己的项目中debug时就会不成功,报错Break at address "0x3fe493" with no debug information available, or outside of program code.

代码如下:把计算函数放在了ADC中断里,怀疑是因为中断嵌套导致函数计算太复杂?

//
// adcA1_ISR —— ADCA Interrupt 1 ISR

//
interrupt void adcA1_ISR(void)

{
    // adcAResults为Digital representation of the voltageon pin Ao

adcAResults = ADC_readResult(ADCARESULT_BASE,ADC_SOC_NUMBERO);

adcAResults1 =  ADC_readResult(ADCBRESULT_BASE,ADC_SOC_NUMBERO);

adcAResults2 = ADC_readResult(ADCCRESULT_BASE,ADC_SOC_NUMBERO);

Pos_calculate(&p);

theta = p.thetaElec;

//Clear INT flag

ADC_clearInterruptStatus(ADCA_BASE,ADC_INT_NUMBER1);

//Check if overflow has occurred

if(true == ADC_getInterruptOverflowStatus (ADCA_BASE,ADC_INT_NUMBER1))

{
    ADC_clearInterruptOverflowStatus(ADCA_BASE,ADC_INT_NUMBER1);

    ADC_clearInterruptstatus (ADCA_BASE,ADC_INT_NUMBER1);
}

// Acknowledge interrupt group

Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);

}

x 出现错误。请重试或与管理员联系。