This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to generate 12 channels of 100kHz PWM signals for controlling the NPC inverter, but the launchpad will not work when I set them to 60kHz. I would like to ask whether launchxl-F28379D can generate 12 channels of 100kHz PWM signals. If not, do I need to use FPGA? Is there any recommended development board? It is best to support code generation.
we discuss in following link: