This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320F28020的烧写问题

Other Parts Discussed in Thread: TMS320F28020

先说下前提:

     需要烧写的目标芯片是TMS320F28020

     仿真器用的是XDS100,在28034能正确连接和烧写,CCS用的最新的CCS3.3,包含2802x系列和2803X系列,但是其中那个选择仿真器的选项中没有28020和28021,只有28022开始的2x系列,  但是GEL文件都有。

然后说下问题:

     用CCS3.3S烧写28020时,选择GEL文件时28020,能正确连接,在选择out文件及配置FLASH  API文件后,点击下载,这时就死在这个界面上,程序下载不进去;

 然后用28021的GEL文件,同样设置后,正确下载,而且程序正确运行;这是什么原因?(用其他芯片的GEL可以,用自己的不可以。。。。。)

    用28021烧写成功后,断电,重新上电,程序有一定几率跑不起来?有时候跑得起来,有时候跑不起来,一开始初步怀疑是bootmode引起的,查看了3个配置引脚,满足getmode模式---跳到flash启动模式;

现在怀疑:28020芯片是否会有这种bug或者一些缺陷?   因为28020的ram只有1k,程序里的变量如果太多,大于1K,是否会影响不能烧写本身的GEL,却能下载28021的GEL或者跑不起来的现象??

请教下TI的专家,这现象的确奇怪,还有我们做了好几块板子,线路,布局都没问题,但是现象都一样。求指导,谢谢~~~~