This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: 程序编译出错,生成的文件大小超过了RAM大小

Part Number: TMS320F28388D


最终的目的是为了使用ethercat从站的功能,使用官方示例中的f2838x_cpu1_echoback_solution这个工程,然后使用SSC tool来生成相应的从站代码,然后将生成之后的工程文件导入到ccs中,点击build之后会报错,提示RAM空间不足,报错提示如下:"../2838x_RAM_lnk_cpu1.cmd", line 67: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".text" size 0x3b52 page 0.  Available memory ranges:。我调整了编译优化等级去优化空间,还是编译不过去。我想知道为什么按照手册来生成从站代码之后工程会变得这么大,我该如何去做修改才能正常使用ethercat从站功能。