如何使PWM1响应TZ1,PWM2响应TZ2,该如何配置。
您说没一个PWM模块可以单独配置,是哪个寄存器设置的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如何使PWM1响应TZ1,PWM2响应TZ2,该如何配置。
您说没一个PWM模块可以单独配置,是哪个寄存器设置的?
有个现象, EPwm1Regs.TZSEL.bit.OSHT1 = 1; EPwm2Regs.TZSEL.bit.OSHT1 = 1; 应该PWM1和PWM2是同样的地位了,即同时响应TZ。我的板子上,有时有PWM2响应TZ输出低电平,而PWM1不响应TZ,这可能是什么原因造成的呢?
你是说有时可以,有时不可以,还是PWM2可以PWM一直不可以?
另外,对应的PWM占空比是多少?有没有将PWM1/2和TZ信号一起抓在示波器上比较一下时序?
同时,可能还需要检查你的PWM设置,除了以上的两句话以外,还有TZCTL寄存器。