提示内容:
Failed Software Reset:
Error 0x00000024/-1137
Error during: Register, Execution,
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings. If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration.
If this is a multi-core system, the master CPU may not be
releasing the DSP/MCU from reset. Please check your
configuration in CC_setup and/or your GEL file to ensure that
nothing is blocking the DSP/MCU from being released from reset
请问会有哪些原因引起该问题,谢谢!!!