Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
你好,提前感谢您能回答,
我在使用基于C2000的F28388D,在simulink使用MBD编译过程中报错。
1. 首先,如下图,报错的内容是:Build process stopped at compile stage. Unable to find the following link-only objects that are specified in the build information: C:\ti\c2000\C2000W~1\DRIVER~1\libraries\math\IQmath\c28\lib\IQmath_fpu32.lib。

我并没有找到报错的该目标路径,因此对于IQmath_fpu32.lib,我找到了其路径:C:\ti\c2000\C2000Ware_5_02_00_00\libraries\math\IQmath\c28\lib,如下图

我在simulink--setting--Code generation--Custom Code--Additional build information--Libraries添加了该路径,如下图,

请问上述操作是否正确?