This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375S: c2000系列生成intel hex格式错误,数据度为0x20,每次换行增加0x10

Part Number: TMS320F28375S


CCS 12编译器 芯片选择为TMS320F28375S芯片,使用生成的out是可以进行烧录的,但是生成的HEX文件格式不对,如图,数据长度为0x20,但是每次换行增加的地址确是0x10。

如图第三行第一个20代表这一行有0x20个字节,地址为0x08,那么第四行应该为0x08+0x20=0x28,但是地址却为0x18,这个问题如何解决呢?

我的猜测是因为28375s的flash一个地址占2个字节,这个如何解决