This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28x_usDelay()



程序为了实现精确的定时,使用了一个用汇编编写的延时函数DSP28x_usDelay(),该函数在文件DSP281x_usDelay.asm中,细节请阅读该文件。为了调用该函数,在Main.c中做了如下声明:

extern void DSP28x_usDelay(Uint32 time);

该函数的定时仍然不够精确,因此在文件DSP281x_Examples.h中做了如下的宏定义修正:

#define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L)

函数DSP28x_usDelay(Uint32 time)要想非常精确,必须在SARAM中运行,因此需要在运行时将其调入SARAM中。为此,需要做如下工作:

首先,在DSP281x_usDelay.asm中使用

.sect "ramfuncs"

将该段代码定义到段“ramfuncs”中,段ramfuncs的位置在编译时指定,实际上由F2812.cmd文件中的如下语句来指定:



ramfuncs LOAD = FLASHD, PAGE = 0,

RUN = RAML0, PAGE = 1,

LOAD_START(_RamfuncsLoadStart),

LOAD_END(_RamfuncsLoadEnd),

RUN_START(_RamfuncsRunStart)



第1行表示该段的装载在PAGA0的FLASHD中(PAGA0和FLASHD的分段请见F2812.cmd文件,后文将有详解);

第2行表示该段的运行地址在PAGE1的RAML0中(PAGA1和RAML0的分段请见F2812.cmd文件,后文将有详解);

LOAD_ START(_RamfuncsLoadStart)令编译器创建了一个变量RamfuncsLoadStart,该变量指向段ramfuncs的装载地址的首地址(LOAD_ START为编译伪指令,请见CCS的帮助文档);

LOAD_ START(_RamfuncsLoadEnd)令编译器创建了一个变量RamfuncsLoadEnd,该变量指向段ramfuncs的装载地址的末地址(LOAD_ END为编译伪指令,请见CCS的帮助文档);

LOAD_ START(_RamfuncsRunStart)令编译器创建了一个变量RamfuncsRunStart,该变量指向段ramfuncs的运行地址的首地址(LOAD_ START为编译伪指令,请见CCS的帮助文档);

从第1和2行可以看出,段ramfuncs中的函数DSP28x_usDelay()的装载地址和运行地址是不同的,本程序中装载在Flash的块FLASHD中,而在SARAM L0中运行,这只是目标,实际运行时DSP并会自动将Flash中的代码拷贝到SARAM中,因此需要手动添加代码来完成。

在C函数中,为了使用变量RamfuncsLoadStart、RamfuncsLoadEnd和RamfuncsRunStart,必须先声明,本工程在文件DSP281x_GlobalPrototypes.h中做了如下声明:

extern Uint16 RamfuncsLoadStart;

extern Uint16 RamfuncsLoadEnd;

extern Uint16 RamfuncsRunStart;

然后就可以使用了。在Main.c中,使用MemCopy()函数将段ramfuncs中的函数DSP28x_usDelay()的代码从装载地址RamfuncsLoadStart—RamfuncsLoadEnd拷贝到RamfuncsRunStart开始的SARAM空间中。之后在程序运行时,只要调用DSP28x_usDelay()函数,都会自动地指向SARAM中相应的函数入口地址,这一点是自动完成的。MemCopy()函数原型在MemCopy.c中,在DSP281x_GlobalPrototypes.h声明。

注意:即使这样,定时仍然可能不精确,因为可能有中断打断DSP28x_usDelay()的运行,所以在调用之前要关中断。