This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320L28034 连不上仿真器



各位好,现在遇到这样一个问题,自制的28034板子突然连不上仿真器,通过SCI boot load 也不能成功。但脱离仿真器上电观察程序应该还是在跑,只是感觉程序执行的非常慢,扫描周期非常的长。所以开始就怀疑是晶振有问题(External Oscillator),换了一个,问题依旧。用示波器测试下X1引脚,发现波形是个频率为739.5Hz 的方波(正常的波形应该是20MHZ的正弦波才对)。测量的波形,晶振电路和晶振配置程序见附件,请各位帮助分析一下,非常感谢! 另外,最后换了新的28034芯片,第一次可以连上仿真器,烧写好程序后问题依旧。 程序烧写的编译连接好目标.out 文件,所以应该不会是程序问题。
28034 连不上仿真器.doc