This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335 用ccs6.0生成bin文件及boot

大家好,我目前正在做f28335的远程升级,方法是自己写一个boot程序,然后用ccs6.0将程序编译后生成bin文件,再通过串口将bin文件发送给boot,最后boot将bin

文件写入F28335的片内flash。

请大家指教这种方式是否正确,以及ccs6.0能否直接生成bin文件。我现在用其它软件将hex文件转换成bin,但是与ccs仿真时读取的片内flash内数据不同,很奇怪。

还请大家多多指教。

  • CCS6.0不能生产BIN文件,至少CCS5.2是不行的,但可以生产hex文件,再解析hex文件就行了,不能用软件转hex,需要自己解析;

    解析可以参考:

    http://wenku.baidu.com/link?url=E1auIQknS_FzkbLP06RXPtdF9v9aP6Dtmi_EdO2Ou-LqQBnZ1T-gIilvU7oytlZgv7Reh9k7NARRvDe4XwBdftk_B78P6Uq0PtrfpAXOuQS

  • 可以这样操作,CCS6.0也可以直接生成hex文件,通过配置工程的build选项直接生成hex文件,如下图:

  • 谢谢!但是,我现在解析的bin文件内容与ccs直接烧写到芯片的内容为什么不一样?

  • 大师,CCStudio6.0如何配置才能使用28335啊,另外,CCS6.0,你有没有破解版的?学习使用,感觉买个软件,忒贵了

  • 大侠是否实现这个远程升级,我现在也想这样做

  • 请问CCS6.2怎么才能生成bin文件?能够直接成成吗,我现在可以生成hex文件,但是想用bootloader把app下载到半板子里貌似要用bin文件。