Part Number: UCD3138
编译环境为CCS10,编译器为ti-cgt-arm_5.2.9,官网下载的例程,编译后报以下错误
#1559 Interrupt handlers must be compiled in ARM mode
如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCD3138
编译环境为CCS10,编译器为ti-cgt-arm_5.2.9,官网下载的例程,编译后报以下错误
#1559 Interrupt handlers must be compiled in ARM mode
如何解决?
这个问题解决了,现在有另一个问题
<Linking>
"C:/ti/DigitalPower/LLCHBFirmware-1.2/Firmware/Device/UCD3138/Linker/cyclone.cmd", line 81: error #10099-D:
program will not fit into available memory. placement with alignment fails
for section ".vectors" size 0x40 . Available memory ranges:
VECS size: 0x20 unused: 0x20 max hole: 0x20
undefined first referenced
symbol in file
--------- ----------------
$c_int00 ./load_UCD3138.obj
在程序中对应问题的代码为
.vectors : {} > VECS
该如何解决?