This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有没有测试TMS320F2812外部SRAM读写速度的简单方法或程序



我做的一块2812的板子项目测试中发现外部SRAM读写速度最快只能达到3.5MHz左右,而资料显示理论上可以达到75MHz。我想独立测试一下这块板子的外部SRAM读写速度,哪位有测试2812外部SRAM读写速度的简单方法或程序?希望不吝赐教。谢谢!

  • 对任何外部空间读/写操作的时序都可以分成3部分:建立、激活和保持,时序如图1和图2所示。在建立(lead)阶段,访问存储空间的片选信号变为低电平并且地址被送到地址总线(XA)上。默认情况下该阶段的时间设置为最大,为6个XTIMCLK周期。在激活(active)阶段,对外部设备进行读写,相应的读写信号(XRD和XWD)变为低电平,同时数据被送到数据总线(XD)上。默认情况下读写该阶段的时间均设置为14个XTIMCLK周期。跟踪(trail)阶段是指读写信号变为高电平,但片选信号仍保持低电平的一段时间周期,默认情况下该阶段时间设置为6个XTIMCLK周期。因此,在编程时要根据外部设备的接口时序来设置XINTF的时序,从而正确地对外设读写。

  • 设定DSP 内核频率(SYSCLK)为120MHz,设定XINTF频率为SYSCLK/2,即60MHz。根据器件手册,IS61LV25616的读/写周期为10ns,因此ZONE2配置为最小的等待时间,建立、激活和跟踪时间分别为16ns、16ns、0ns,写信号周期为16ns、16ns、0ns(对应寄存器设置为1,1,0)。AT28LV256的读写时序如图4、图5所示,读信号周期:建立时间为tCE与tOE之差,最大值为120ns;激活时间为tOE,最大值为80ns;跟踪时间为tOH,最大值为0,因此配置为33ns、50ns、0ns(对应寄存器设置为1,2,0)。写信号周期:建立时间为tCS,最小值为0;激活时间为tWP,最小值为200ns;跟踪时间为tCH,最小值为0ns。因此配置为33ns、217ns、33ns(对应寄存器设置为1,6,1)。