This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335里如何实现printf输出



我用的芯片28335,CCS5.4。

我想用printf在console里打印数据,老是不成功。

我的程序:

#include"DSP2833x_Device.h" #include"math.h" #include"stdio.h"  float spo,spe;

void main(void) {  float j;  float k;     int a;     int b;

    a=1413;     b=12412;     j=123.56;     k=323.41;     spo=(float)a*b;  spe=(j+k)*j/k;  printf("xzz");  while(1); }

 CMD文件如下:

MEMORY { PAGE 0 :    /* BEGIN is used for the "boot to SARAM" bootloader mode      */

   BEGIN      : origin = 0x000000, length = 0x000002     /* Boot to M0 will go here                      */    RAMM0      : origin = 0x000050, length = 0x0003B0    RAML0      : origin = 0x008000, length = 0x001000    RAML1      : origin = 0x009000, length = 0x001000    RAML2      : origin = 0x00A000, length = 0x001000    RAML3      : origin = 0x00B000, length = 0x001000    ZONE7A     : origin = 0x200000, length = 0x00FC00    /* XINTF zone 7 - program space */    CSM_RSVD   : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */    CSM_PWL    : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA            */    ADC_CAL    : origin = 0x380080, length = 0x000009    RESET      : origin = 0x3FFFC0, length = 0x000002    IQTABLES   : origin = 0x3FE000, length = 0x000b50    IQTABLES2  : origin = 0x3FEB50, length = 0x00008c    FPUTABLES  : origin = 0x3FEBDC, length = 0x0006A0    BOOTROM    : origin = 0x3FF27C, length = 0x000D44

   RAML6L7    : origin = 0x3F8000, length = 0x003000

PAGE 1 :    /* BOOT_RSVD is used by the boot ROM for stack.               */    /* This section is only reserved to keep the BOOT ROM from    */    /* corrupting this area during the debug process              */

   BOOT_RSVD  : origin = 0x000002, length = 0x00004E     /* Part of M0, BOOT rom will use this for stack */    RAMM1      : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */    RAML4      : origin = 0x00C000, length = 0x001000    RAML5      : origin = 0x00D000, length = 0x001000

   ZONE7B     : origin = 0x20FC00, length = 0x010400     /* XINTF zone 7 - data space */    ZONE7C     : origin = 0x22FC00, length = 0x010400    ZONE7D     : origin = 0x24FC00, length = 0x010400 }

SECTIONS {    /* Setup for "boot to SARAM" mode:       The codestart section (found in DSP28_CodeStartBranch.asm)       re-directs execution to the start of user code.  */    codestart        : > BEGIN,     PAGE = 0    ramfuncs         : > RAML0,     PAGE = 0    .text            : > RAML6L7,   PAGE = 0    .cinit           : > RAML0,     PAGE = 0    .pinit           : > RAML0,     PAGE = 0    .switch          : > RAML0,     PAGE = 0

   /*.stack           : > RAMM1,     PAGE = 1    .ebss            : > RAML4,     PAGE = 1*/    .stack           : > ZONE7C,     PAGE = 1    .ebss            : > ZONE7D,     PAGE = 1    .econst          : > RAML5,     PAGE = 1    .esysmem         : > RAMM1,     PAGE = 1

   .cio    : > RAML5,   PAGE = 1

   IQmath           : > RAML1,     PAGE = 0    IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD

   /* Uncomment the section below if calling the IQNexp() or IQexp()       functions from the IQMath.lib library in order to utilize the       relevant IQ Math table in Boot ROM (This saves space and Boot ROM       is 1 wait-state). If this section is not uncommented, IQmathTables2       will be loaded into other memory (SARAM, Flash, etc.) and will take       up space, but 0 wait-state is possible.    */    /*    IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD    {

              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

   }    */

   FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

   DMARAML4         : > RAML4,     PAGE = 1    DMARAML5         : > RAML5,     PAGE = 1    //DMARAML6         : > RAML6,     PAGE = 1    //DMARAML7         : > RAML7,     PAGE = 1

   ZONE7DATA        : > ZONE7B,    PAGE = 1

   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used                    */    csm_rsvd         : > CSM_RSVD   PAGE = 0, TYPE = DSECT /* not used for SARAM examples */    csmpasswds       : > CSM_PWL    PAGE = 0, TYPE = DSECT /* not used for SARAM examples */

   /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */    .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD

}

请高手指教,谢谢!