Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 6.2.4 [C2000]. Another version of the compiler will be used during build: 6.4.2. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. HVLLC properties Problems今天编译的是后出现一个这样的警告,请问到哪里下载?我昨天也是这样编译,但是没出现这个警告。