This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
新装的CCSV6.1,编译28035程序提示错误,错误如下:
[MEMORY.]
>> WARNING: invalid compiler option --l2803x_FlashAPI_BootROMSymbols.lib(.text) (ignored)
>> WARNING: more than one source file is specified; preprocessor output will be generated for last file only
Fatal error #1965: cannot open source file "MEMORY"
1 catastrophic error detected in the compilation of "MEMORY".
Compilation terminated.
请专家指点一下,谢谢!
我用的CCS Version: 6.1.0.00104导入controlSUITE中 F28035例程(不选copy project),编译是成功的。
你也试一下?
建议你先直接导入controlSUITE里面自带的28035的工程
然后右键工程在特性下 设置Device型号 进行编译看看有没有问题
如果没有问题 就可以排除CCS安装问题