我现在做谐波分析,要首先AD采样,遇到两个问题:
1、采样频率设置问题,我想是频率分辨率为5,又考虑采样定理所以决定设置采样频率为10240Hz,采样点数为2048.我的采样率是epwm触发的,但是发现如果设置10240那么寄存器PRD赋值需要是小数,这个没法完成,但是确实看到论文中有这样的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在做谐波分析,要首先AD采样,遇到两个问题:
1、采样频率设置问题,我想是频率分辨率为5,又考虑采样定理所以决定设置采样频率为10240Hz,采样点数为2048.我的采样率是epwm触发的,但是发现如果设置10240那么寄存器PRD赋值需要是小数,这个没法完成,但是确实看到论文中有这样的。
如果要设置频率是10240Hz,那么周期就要精确到皮秒了,而150M的分辨率是6.67ns,所以是肯定无法设置到这个频率上的。
修改cmd文件,比如:
FLASHM : origin = 0x102000, length = 0x002000 /* on-chip FLASH */
FLASHL : origin = 0x104000, length = 0x002000 /* on-chip FLASH */
FLASHK : origin = 0x106000, length = 0x002000 /* on-chip FLASH */
如果数组放在M里面不够,可以改为:
FLASHM : origin = 0x102000, length = 0x004000 /* on-chip FLASH */
FLASHK : origin = 0x106000, length = 0x002000 /* on-chip FLASH */