DSP2812开发板与仿真器连接的时候出现错误:
Failed Software Reset: Error 0x00000020/-1150 Error during: Execution, JTAG protocol reset. Sequence ID: 17 Error Code: -1150 Error Class: 0x00000020
Trouble Reading PC Register: Error 0x00000004/-1166 Error during: Register, Lost processor clock. Device may be operating in a low-power mode. Do
you want to bring it out of this mode? Sequence ID: 5 Error Code: -1166 Error Class: 0x00000004
GEL: Error while executing OnReset(1): target is not connected.
Failed Software Reset: Error 0x00000020/-1150 Error during: Execution, JTAG protocol reset. Sequence ID: 17 Error Code: -1150 Error Class: 0x00000020
Can't Run Target CPU: Error 0x00000020/-1150 Error during: Execution, JTAG protocol reset. Sequence ID: 13 Error Code: -1150 Error Class: 0x00000020
请问怎么解决?谢谢啦!