This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于SOLAR例程中数字反馈环的一些疑问



哦最近在做一个逆变器的项目,阅读TI的例程时碰到一些问题,请教大家:

问题1:在SolarExplorer_v1.0例程项目的SolarExplorer-Main.c中电流内环PID_GRANDO的系数为:

             pidGRANDO_Iinv.param.Kp=0.8;
             pidGRANDO_Iinv.param.Ki=(0.15);
             pidGRANDO_Iinv.param.Kd=(0.0);

            电压外环的的PID_GRANDO的系数为:

             pidGRANDO_Vinv.param.Kp=(3.0);

             pidGRANDO_Vinv.param.Ki=(0.005);

             pidGRANDO_Vinv.param.Kd=(0.0);

             Kd=0表示为PI调节器,Kp、Ki的系数如何计算得到,我看了例程项目下的PDF文档也还是不清楚,请问可以提供详细一点的说明吗?

问题2:HV_SOLAR_DC_AC_v1.1例程项目的Solar_HV_DCAC_Concerto_C28.c中电流内环没有使用PID_GRANDO,而是用的CNTL_2P2Z,系数为:

             CNTL_2P2Z_CoefStruct2.b2 = _IQ26(-0.3938);

             CNTL_2P2Z_CoefStruct2.b1 = _IQ26(0.1314);
             CNTL_2P2Z_CoefStruct2.b0 = _IQ26(0.5253);
             CNTL_2P2Z_CoefStruct2.a2= _IQ26(-0.01);
             CNTL_2P2Z_CoefStruct2.a1= _IQ26(1.01);
             CNTL_2P2Z_CoefStruct2.max = _IQ24(0.4);
             CNTL_2P2Z_CoefStruct2.min = _IQ24(-0.4); //400

             我已了解PID的系数与2P2Z可以相互转换,我想问什么情况下使用PID_GRANDO,什么情况下使用CNTL_2P2Z。而且2P2Z的系数在文档中也未提及

如何得到,有相关资料介绍的详细一些吗?

问题3:在SLOAR_V1.2中已提供CNTL_2P2Z_F函数,而F28M35支持浮点计算,为什么例程中仍使用CNTL_2P2Z及Q格式的浮点数呢?

              请大家不吝指教,先谢谢了!