This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如何用dsp28035来采样交流电压
你需要先把交流电压进行分压至-1.65V ~1.65V,然后通过一个运放增加1.65V偏置,使得最后的输出是0-3.3V,在F28035的AD口前增加RC低通滤波器以及二极管钳位电路作为保护。你也可以直接采用隔离运放 直接偏置到0-3.3V。
那如何通过采样值,来分析电压的频率、有效值
频率需要分压后使用比较器,输入给内部ECAP来捕捉,有效值就是峰峰值的2^1/2
就是说,分压后,使用过零比较器,产生方波,捕获周期,即可得交流电压频率。那最大值就是通过adc在一个周期内多次采样比较,得到最大值,是这样理解的吗
再请教一个问题,那交流电流的频率,有效值有如何采样
电流的频率和电压是一样的,不需要采样,有效值就是你采出来的幅值的1/根号2