This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2812与ADS1118通讯时有问题?

Other Parts Discussed in Thread: ADS1118

#include "DSP281x_Device.h"
#include "DSP281x_Spi.h"
#include "DSP281x_Delay.h"

#define  CS  GpioDataRegs.GPFDAT.bit.GPIOF3

void InitSPI(void)
{
    EALLOW;
    GpioMuxRegs.GPFMUX.all = 0x0007;

    GpioMuxRegs.GPFDIR.all |= 0x0008; //把STEA设置成普通IO模式
    EDIS;
    //使用的是普通SPI模式,没用FIFO
    SpiaRegs.***.bit.SPISWRESET=0; // Reset SPI
    SpiaRegs.***.all=0x0007;       // 8-bit character, Loopback mode disabled*数据是8位
    SpiaRegs.***.all=0x0006;       // SPI Interrupt disabled, Master mode, Master/slave transmit enabled  主模式
    SpiaRegs.SPISTS.all=0x0000;       //状态位清零
    SpiaRegs.SPIBRR=127;           //计算波特率 LSPCLK/(SPIBRR+1)=30/127+1=234
    //SpiaRegs.SPIPRI.all=0x0040;
    SpiaRegs.***.all=0x0087; // Enable SPI
}

/************************************************
0x058B  A0/A1    +/-2.048   0x038B  A0/A1    +/-4.096
0x458B  A0/GND   +/-2.048   0x438B  A0/GND   +/-4.096
0x558B  A1/GND   +/-2.048   0x538B  A1/GND   +/-4.096
0x658B  A2/GND   +/-2.048   0x638B  A2/GND   +/-4.096
0x758B  A3/GND   +/-2.048   0x738B  A3/GND   +/-4.096
**********************************************/
void ADS_Config(void)
{
        unsigned int Config_Value;
        Config_Value = 0x538B; // ADS1118 configuration AIN1, FS=+/-4.096, DR=128sps, PULLUP on DOUT
        CS=0;                        // Set CS low
        WriteSPI(Config_Value,0);    // Write configuration to ADS1118
        CS=1;                        // Set CS high
}
int ADS_Read(void)
{
        unsigned int Data, Config_Value;
        Config_Value = 0x538B;// ADS1118 configuration AIN1, FS=+/-4.096, DR=128sps, PULLUP on DOUT
        CS=0;                         // Set CS low
        Data = WriteSPI(Config_Value,1);   // Read data from ADS1118
        CS=1;                           // Set CS high

        return Data;
}

/*
* Mode 0: Only write config register to ADS1118
* Mode 1: Write config register to ADS1118 as well as read data from ADS1118
*/
signed int WriteSPI(unsigned int config, unsigned char mode)
{
        signed int msb,TEMP_dummy;
        unsigned int temp;
        volatile signed int dummy;

                temp = config;
        if (mode==1) temp = config | 0x8000;

        while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG==1);     //判断是否发送完毕
        SpiaRegs.SPITXBUF = (temp >> 8 );              // Write MSB of Config
         while(SpiaRegs.SPISTS.bit.INT_FLAG ==0);
         msb = SpiaRegs.SPIRXBUF;                      // Read MSB of Data

        while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG==1);
        SpiaRegs.SPITXBUF = (temp & 0xff);            // Write LSB of Config
        while(SpiaRegs.SPISTS.bit.INT_FLAG ==0);
        msb = (msb << 8) | SpiaRegs.SPIRXBUF;          // Read LSB of Data

         while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG==1);
         SpiaRegs.SPITXBUF = (temp >> 8 );             // Write MSB of Config
         while(SpiaRegs.SPISTS.bit.INT_FLAG ==0);
         dummy = SpiaRegs.SPIRXBUF;                     // Read MSB of Config


        while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG==1);
        SpiaRegs.SPITXBUF= (temp & 0xff);                // Write LSB of Config
        while(SpiaRegs.SPISTS.bit.INT_FLAG ==0);
        TEMP_dummy=dummy;
        dummy = (TEMP_dummy <<8) | SpiaRegs.SPIRXBUF;  // Read LSB of Config

        delay_us(100);

        return msb;
}