This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关于CONTROLSUITE中HVPM2833xSENSORLESS例程的请教



各位大神想问下,HVPM2833Xsensorless的level1是开环控制,我看内个TI出的内个说明书说是LEVEL1不接电机,但是如果我接上电机是不是应该也是可以转的?

  • 你好。

    LEVEL1是完全开环的,但是可以发出来SVPWM。给定的变量是转速、D轴和Q轴的电压(注意这里的D和Q不是实际电机的D和Q轴,分析一下就可以知道了)。

    LV1和LV2的差别在于,LV1只发波,不采样,LV2加上了AD采样。

    所以,LV1接上电机也是可以转的。

  • Jay 说:

    你好。

    LEVEL1是完全开环的,但是可以发出来SVPWM。给定的变量是转速、D轴和Q轴的电压(注意这里的D和Q不���实际电机的D和Q轴,分析一下就可以知道了)。

    LV1和LV2的差别在于,LV1只发波,不采样,LV2加上了AD采样。

    所以,LV1接上电机也是可以转的。

    您好,我还想问一下,这种开环没有反馈的控制,PWM波形的占空比是如何给定的呢。。。?