This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335



最近在使用F28335-AD模块,但是对AD模块的配置有些迷惑和问题,请大神介绍一下配置思路,帮忙理清一下。

1、配置思路,(触发和时钟就不用说啦)

2、问题,我在运行程序时 ,明明是配置的 adcresult0,却在其他的adcresult0出现值

3、我采样的电压最大为3.12v,会烧毁AD模块吗

问题有点多,麻烦大家啦

  • 1、配置采样时钟速率,转换方式设定,采样通道分配,使能启动模式,使能中断模式,差不多就是这几步

    2、adcresult0对应的是采样通道0所配置的引脚。不过你所说好像是同一个寄存器啊?

    3、28335电压范围:0-3V,但是数据表中有≥3V,数字值为4095的描述,感觉会有点余量,到底有多少余量不知道。有可能和接入的模拟电源有关。烧不烧毁不说,至少你那么高的电压是没有意义的。