This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error 0x00000220/-1166 解决方案



Error connecting to the target: Error 0x00000220/-1166 Error during: Execution, OCS,  Lost processor clock. Device may be operating in a low-power mode.  Do you want to bring it out of this mode?   Sequence ID: 0 Error Code: -1166 Error Class: 0x00000220
Error connecting to the target: Error 0x00001200/-1166 Error during: OCS, Target,  Lost processor clock. Device may be operating in a low-power mode.  Do you want to bring it out of this mode?   Sequence ID: 0 Error Code: -1166 Error Class: 0x00001200

 

出现上述错误,调整f2812无源晶振两侧滤波电容值,改为20pf或者22pf。

主要是dsp晶振问题。

 

根据个人经验    出现连接等问题      如果确保仿真器和仿真器驱动安装合适的话     

首先检查电源      即内核电压和IO电压    是否在合理的范围内

电源没有问题    就用示波器检查芯片的CLKOUT引脚     此引脚有固定频率的波形输出

那就说明芯片工作是正常的。