This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

rts2800_fpu32.lib和rts2800_ml.lib的区别?

哪位大神,可以告诉我rts2800_fpu32.lib和rts2800_ml.lib的区别?用28335实现浮点运算是不是调用rts2800_fpu32.lib,然后在build options中选择支持32位浮点运算就可以了吗?这样是不是就用到了了28335的浮点运算核,还有没有其他方法进一步加快运算速度?

  • rts2800_fpu32.lib是浮点FPU支持库,rts2800_ml.lib是定点支持库。调用rts2800_fpu32.lib,然后在build options中选择支持32位浮点运算,编译时就会将相关的浮点运行函数编译成浮点指令,通过F28335的FPU来执行。

  • Hank Zhao :

          您好,您的意思是这样就加入了F28335的FPU,浮点运算速度已经达到了最快?那还有没有其他方法加快浮点运算,比如CLAmath?CLAmath还可以加快吗?谢谢!

  • 这样就可以把C代码中的浮点算法编译成浮点指令,F28335没有CLA模块,不能使用CLAmath。如果想进一步优化浮点算法,你可以把rts2800_fpu32_fast_supplement.lib添加到工程中去。

  • 您好:

           rts2800_fpu32_fast_supplement.lib添加到工程中去,CCS还需不需其他设置呢?谢谢您。

  • 在工程properties--build--link order中用“up”“down”按钮改变一下两个库的位置,保证fast library在上方,这样会优先调用fast library中的函数,其它的设置不需要改变。

  • 你好!我有相关问题请教一下。我已经按照相关要求进行如下配置: 1 in Runtime Model Options, under "Specify floating point support (--float_support) pull-down menu: Select "fpu32". 2 In "Include linker file or command file as input (--library, -l)"box, click green plus sign and add rts2800_fpu32.lib(run-time support library). 但是,编译工程后,警告我“function sin declared implicitly”,并且计算结果也是错的。请问是什么情况?谢谢你!
  • 请您将您的问题详细描述后重新发帖,请不要跟踪旧贴,谢谢